Technical FAQs

Ask a Question

Do we have an overcurrent fault on the Altivar ATV56?

The drive measures output current and faults either on motor overload, based on motor FLA, short circuit fault, or ground fault.


CTA-ID : 6763
Was this helpful?
What can we do to improve the information ?