Technical FAQs

Ask a Question

Do you have to size the line reactor based on motor hp or Altivar ATV56 drive hp?

The line reactor will have to be sized for the drive hp. Also provide external motor overloads if the motor fla is below 45% of the drive controller rating.

CTA-ID : 6757
Was this helpful?
What can we do to improve the information ?