Technical FAQs

Ask a Question

Can the Altivar ATV56 drive run in Reverse?

There is a way to make the drive run in reverse by using Rev Speed function under the Setpoint Manual parameter. Also if AI2 is multiplied by -1 and the sum is a negative no., also if Clamp Sum is set to NO then the drive will reverse direction.


CTA-ID : 6717
Was this helpful?
What can we do to improve the information ?