Technical FAQs

Ask a Question

Can you run the ATV56 unit in Keypad command.

You need to program the ( Ter/Key by LI.... ) in menu 5.0 Highlight that parameter and enter. Select Lix (desired logic inoput) and hit enter. Then to put it into keypad mode close a contact between LIx (logic input selected) and +24.



CTA-ID : 6691
Was this helpful?
What can we do to improve the information ?