Technical FAQs

Ask a Question

If you have a Square D Thermal magnetic circuit breaker on line side of ATV18 drive do you still need fuses?

Yes. Fuses are needed to protect from ground fault/short circuit currents. They are coordinated with the fault withstand rating of the drive. The circuit breakers are not fast enough.


CTA-ID : 6676
Was this helpful?
What can we do to improve the information ?