Technical FAQs

Ask a Question

Is the basic Altivar ATV18 in a NEMA 1 enclosure?

No the basic ATV18 is rated NEMA Open (IP31/IP20). Would have to order an enclosed ATV18 in order to get a NEMA 1 enclosure.

CTA-ID : 4401
Was this helpful?
What can we do to improve the information ?