Technical FAQs

Ask a Question

What is the ambient temperature the Altivar ATV18 drive can run in?

Issue: What is the ambient temperature the Altivar ATV18 drive can run in?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: The maximum ambient temperature is 104 deg F without the grey tape removed. The maximum ambient temperature with the grey tape removed is 122 deg F. The degree of protection goes from IP31 to IP20 when the grey tape is removed.


 
Was this helpful?
What can we do to improve the information ?