Technical FAQs

Ask a Question

What is the part number for a replacement load base assembly for a D325N General Duty safety switch?

The part number will depend on the Series number of the safety switch. For a Series E3, use 4051062850,. For Series E2 or E1, use 4051046550. For  Series D2 (this part is Obsolete and No Longer Available -4051035050).  All Load Base assembly parts for Series prior to D2 are Obsolete and No Longer Available.


CTA-ID : 5647
Was this helpful?
What can we do to improve the information ?