Technical FAQs

Ask a Question

How does the T fuses install in the D325NT, D325NTR, D326NT, D326NTR, T327N, T327NR, general duty safety switches?

Issue:
Product design features

Product Line:
General Duty Safety Switches

Cause:
Fuse installation

Resolution
The 300V, class T fuses are bolt-in type fuses and will bolt into the switches. They are not Plug-in type fuses, so the switches DO NOT contain Jaws.


CTA-ID : 2323
Was this helpful?
What can we do to improve the information ?