Technical FAQs

Ask a Question

What type of fuses fit into the D325NT, D325NTR, D326NT, D326NTR, T327N, T327NR?

Issue:
Application

Product Line:
GD SS

Cause:
Fuse selection

Resolution:
The fusible safety switches accept ONLY Class T, 300 Volt AC fuses.
The D325NT and D325NTR accept 201A - 400A fuses. Check with a fuse manufacturer for availability of specific fuse ampere ratings.
The D326NT and D326NTR accept 401A - 600A fuses. Check with a fuse manufacturer for availability of specific fuse ampere ratings.
The T327N and T327NR accept 601A - 800A fuses. Check with a fuse manufacturer for availability of specific fuse ampere ratings.


CTA-ID : 2317
Was this helpful?
What can we do to improve the information ?