Technical FAQs

Ask a Question

Does the NW Micrologic trip unit require an external power source?

Current-based protection functions require no auxiliary power source.
When an external power supply is added, the value of the interrupted current is stored by the trip unit. The reset button resets alarms, and stored interrupted current indications are maintained.

CTA-ID : 8770
Was this helpful?
What can we do to improve the information ?