Technical FAQs

Ask a Question

What are the repair parts for an EZM742400R, Series 002, Branch Unit?

Issue:
Old design repair parts

Product Line:
EZM Metering

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable:

Parts include Meter Socket through Tenant Circuit Breaker Compartment, include quantities for one position only (where a part number only is given the order quantity for that part is one):

7-Jaw Meter Socket (Lever Bypass Type with Jaw Release, 5th Jaw Wire included) - 61357 - Obsolete, NLA, with No Replacement
Mounting Screws for Meter Socket base - (3) 2149020181
Short Conn. for Line Side and Load Side of Meter Socket - (6) 4052769501 - Obsolete, NLA, with No Replacment
Keps Nuts for Short Line Side and Load Side Connectors - (9) 2342702200
Circuit Breaker - LAL36400

OTHER Available Parts for this device:
Cover Mounting Screw - 4020513002K
Individual Meter Socket Trim (Ringless Type) - 4052789150 - Obsolete, NLA, with No Replacement
Gasket for Meter Socket Trim (Left and Right edges full length) - 1561042401


CTA-ID : 8320
Was this helpful?
What can we do to improve the information ?