Technical FAQs

Ask a Question

What are the repair parts for an EZM542400R, Series 002, Branch Unit?

Issue:
Old Design repair parts

Product Line:
EZM

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable:

Parts include Meter Socket through Tenant Circuit Breaker Compartment, include quantities for one position only (where a part number only is given the order quantity for that part is one):
5-Jaw Meter Socket (Lever Bypass Type with Jaw Release) - 62902
Fifth Jaw Wire for Meter Socket - 4052765850
Mounting Screws for Meter Socket base - (3) 2149020181
Short Conn. for Line Side and Load Side of Meter Socket - (4) 4052769501 - Obsolete, NLA, with No replacement
Keps Nuts for Short Line Side and Load Side Connectors - (4) 2342702200
Circuit Breaker - LAL26400

OTHER Available Parts for this device:
Cover Mounting Screw - 4020513002K
Individual Meter Socket Trim (Ringless Type) - 4052789150 - Obsolete, NLA< with No replacement
Gasket for Meter Socket Trim (Left and Right edges full length) - 1561042401



CTA-ID : 8313
Was this helpful?
What can we do to improve the information ?