Technical FAQs

Ask a Question

What type of electrical protection is required for the fans on Instrument Fans?

While the fans do have internal protection for thermal overload, the control circuit should be properly protected. Should it`s overload protection trip due to mechanical blockage, the fan can restart upon clearing the condition.

CTA-ID : 7638
Was this helpful?
What can we do to improve the information ?