Technical FAQs

Ask a Question

What is the wire binding torque for the GC-200 and GC DSP ground fault relay system?

#24-#14 copper only, twisted pair recommened.
Torque the wiring binding screws to 6-15 lb in. (0.7 - 1.7 NM)
Wire strip length is 0.25 in (6mm)


CTA-ID : 8008
Was this helpful?
What can we do to improve the information ?