Technical FAQs

Ask a Question

What is the instantaneous function on an electronic trip unit?

The instantaneous feature sets a current level above which tripping occurs with no intentional delay. On some circuit breakers, it may be turned off or be absent when the short-time function is used.

CTA-ID : 8738
Was this helpful?
What can we do to improve the information ?