Technical FAQs

Ask a Question

What are the dimensions for the GC-200 and GC DSP ground fault relay system?

Relay: 6.3in W x 3.54in H x 2.28in D; 35 mm DIN rail mountable.
Display: 4.5in W x 4.4in H x 1.25in D; flush mounts over meter cutout.


CTA-ID : 8005
Was this helpful?
What can we do to improve the information ?