Technical FAQs

Ask a Question

What is the required input power supply voltage for the GC-200 ground fault system?

Either 120 Vac (+20/-45%) or 24Vdc (?15); 15W can be used.


CTA-ID : 7995
Was this helpful?
What can we do to improve the information ?