Technical FAQs

Ask a Question

Is there a dimensional difference between the obsolete CJ and the current NSJ?

Yes there are dimensional differences. The CJ400/600/N/H is 12.59 x 6.20 x 4.53, CJ400L is 12.54 x 6.20 x 7.48. Whereas the NSJ400/600/N/H/L is 13.39 x 5.51 x 4.32.

CTA-ID : 7992
Was this helpful?
What can we do to improve the information ?