Technical FAQs

Ask a Question

How is the Long Time (current rating) of an NW/NT breaker with the Micrologic trip unit determined?

Long Time setting determined

Product Line:
Circuit Breakers

Applies to NW/NT breakers with micrologic trip units.

Need to clarify or know what long time setting is set at?

The current rating (Ir ) is the long-time pickup setting multiplied by the sensor plug amperage (In ). If the current exceeds this value for longer than the long-time delay time, the circuit breaker will trip.

CTA-ID : 7986
Was this helpful?
What can we do to improve the information ?