Technical FAQs

Ask a Question

Are ground-fault pickup levels a function of the sensor, sensor plug, or rating plug on new Micrologic trip units?

Ground-fault pickup values (Ig ) are based on circuit breaker sensor plug (In ) only, not on the rating plug multiplier (Ir ). Changing the rating plug multiplier has no effect on ground-fault pickup values.

CTA-ID : 7985
Was this helpful?
What can we do to improve the information ?