Technical FAQs

Ask a Question

When is an auxiliary power supply needed for the new Micrologic x.0 trip units?

Current-based protection functions require no auxiliary power source.
When an external power supply is added, the value of the interrupted current is stored by the trip unit. The reset button resets alarms, and stored interrupted current indications.

CTA-ID : 7976
Was this helpful?
What can we do to improve the information ?