Technical FAQs

Ask a Question

What are the LS0 trip unit functions on a new Micrologic trip unit?

LS0 = Long-time + Short-time with zero delay + Instantaneous. Available on the IEC Rated 2.0 and 2.0A trip units.




CTA-ID : 7965
Was this helpful?
What can we do to improve the information ?