Technical FAQs

Ask a Question

What is the wire range for the 36699 lug for the CJ breaker?

1 - #2/0 AWG to 600 kcmil Cu or #4/0 AWG to 500 kcmil Al.


CTA-ID : 8225
Was this helpful?
What can we do to improve the information ?