Technical FAQs

Ask a Question

What is the part number for directory cards for NQOD panelboards?

The standard directory cards that fit into the plastic pocket and are numbered 1-42 are part number 80031-158-01. The directory cards that are numbered 43-96 are part number 80031-158-02.



CTA-ID : 8626
Was this helpful?
What can we do to improve the information ?