Technical FAQs

Ask a Question

What is the wire range for the 36702 lug for the CJ breaker?

1 - #2/0 AWG to 500 kcmil Cu or
1 or 2 - #2/0 AWG to 350 kcmil Cu or
1 or 2 - #4/0 AWG to 500 kcmil Al



CTA-ID : 8224
Was this helpful?
What can we do to improve the information ?