Technical FAQs

Ask a Question

What are the repair parts for a QO342M225RB, Series S1, Load Center?

Only the parts listed below are considered field replaceable.
Cover - 4056305550
Interior Trim - 4056305401
Interior Assembly - QO342M225RBI
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - KDL32225 (OBSOLETE WITHOUT REPLACEMENT)
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screw - 2142717161
Main Lug Mounting Keps Nut - 2342702001
Main Circuit Breaker Connecting Strap - 4055901901


CTA-ID : 7900
Was this helpful?
What can we do to improve the information ?