Technical FAQs

Ask a Question

What is a QOM22225NRB?

Issue:  
Does the QOM22225NRB come with a breaker installed?

Product line:  
Enclosed circuit breakers

Environment:  
QOM2 circuit breaker enclosures

Resolution:  
A QOM22225NRB is a General Purpose, NEMA (and UL) Type 3R Rainproof enclosure for a QOM2 frame of circuit breaker.  The circuit breaker must be purchased separately.  
Was this helpful?
What can we do to improve the information ?