Technical FAQs

Ask a Question

What is the contact gap for the C60 range when the breaker is open?<br />

The gap between the contacts for the C60 range when the breaker is open is minimum = 5.5 mm. The IEC standard requires 4 mm.


CTA-ID : 8572
Was this helpful?
What can we do to improve the information ?