Technical FAQs

Ask a Question

Is an IEC 947-3 listed non-automatic switch available in the Masterpact NW frame?<br />

Yes. An automatic switch is available with UL 489 and IEC 947-3 listings.
A non-automatic switch is available with ANSI C37 certification, UL 1066 Listing, and with IEC 947-3 listing.


CTA-ID : 7851
Was this helpful?
What can we do to improve the information ?