Technical FAQs

Ask a Question

What range of sensor plugs are avilable for the 1600A NW with UL 489 or UL 1066 / ANSI ratings?

The following amperages are available: 800, 1000, 1200, 1600


CTA-ID : 7798
Was this helpful?
What can we do to improve the information ?