Technical FAQs

Ask a Question

What are the repair parts for a QO318L200GRB, Series S1, Load Center?

Only the parts listed below are considered field replaceable.
Cover - 4054802204
Interior Trim - 4054520301
Interior Assembly - QO318L200RBI
Neutral Bonding Screw - 4028344850K
Main Lugs - QOL3225
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screw - 2142717161
Main Lug Mounting Keps Nut - 2342702000
Equipment Ground Bar - PK23GTA and LK100AN

CTA-ID : 7867
Was this helpful?
What can we do to improve the information ?