Technical FAQs

Ask a Question

What input devices can I use to control Instrument Fans?

The fans must be controlled externally; they will run when power is applied. Additionally, the fans have internal thermal overload. Should it`s overload protection trip due to mechanical blockage, the fan can restart upon clearing the condition.

CTA-ID : 7637
Was this helpful?
What can we do to improve the information ?