Technical FAQs

Ask a Question

Why can`t a 9001 K or 9001 SK illuminated operator be ordered with a shallow depth light module and contacts mounted on both sides?

There are no provisions for mounting contacts behind the shallow depth light module, so contacts can only be mounted beside the shallow depth light module. It was originally developed so an illuminated push button could be mounted in a 9001 SKYP pendant station.

CTA-ID : 8156
Was this helpful?
What can we do to improve the information ?