Technical FAQs

Ask a Question

Why can't a 9001KT Push to Test pilot light be ordered with a shallow depth light module?

Issue:
Why can't a 9001KT Push to Test pilot light be ordered with a shallow depth light module?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product selection

Resolution:
This configuration is not available from Square D as an assembly due to non-conforming wiring issues. Users may obtain this functionality by purchasing a 9001 K2L, the 9001 KM shallow depth light module and the desired lens and assembling the device themselves. Or, if the quantities are sufficient, the sales person may submit a request for an assembled product via the Form.


CTA-ID : 8153
Was this helpful?
What can we do to improve the information ?