Technical FAQs

Ask a Question

Is a UL 1066 / ANSI rated automatic switch available in the Masterpact NW frame?

No. An automatic switch is available with UL 489 and IEC 947-3 listings.
A non-automatic switch is available with ANSI C37 certification, UL 1066 Listing, and with IEC 947-3 listing.

CTA-ID : 7831
Was this helpful?
What can we do to improve the information ?