Technical FAQs

Ask a Question

What types of loads does the 30A flourescent rating of a Class 8903 Type L include?

Issue:
What types of loads does the 30A flourescent rating of a Class 8903 Type L include?

Product Line:
NEMA Lighting Contactors

Environment:
Products sold and used in the United States

Cause:
selecting lighting contactors for the correct load

Resolution:
It includes ballast loads like your standard office lighting. We cannot state that these contactors are approved for use on HID, metal hallide, high pressure sodium, or mercury vapor lighting because NEMA has not developed any standards for them.


CTA-ID : 8150
Was this helpful?
What can we do to improve the information ?