Technical FAQs

Ask a Question

What are the repair parts for a QO1816M150FTRB, Series S1, Load Center?

Only the parts listed below are considered field replaceable.
Cover - 4054802204
Interior Trim - 4056309601
Interior Assembly - QO1816M150FTRBI
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2150VH
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screw - 2142717161
Main Circuit Breaker and Main Lugs Keps Nuts - 2342702001


CTA-ID : 7795
Was this helpful?
What can we do to improve the information ?