Technical FAQs

Ask a Question

What are the repair parts for a 92446 Series E1 Double throw Safety Switch?

The parts listed here are the only field replaceable parts.
Blade assembly - 40538-266-50 (does not include lugs)
Top switch base assembly - 40538-269-50 (does not include lugs)
Bottom switch base assembly - 40538-269-50 (does not include lugs)
Handle knob assembly - 40513-001-50
Lug assembly - 8011612250 (one lug per blade and base assembly)
Keps nut for mounting lugs - 23427-028-00 (one nut per lug)
base mounting screws - 40206-009-01


CTA-ID : 8101
Was this helpful?
What can we do to improve the information ?