Technical FAQs

Ask a Question

What is included in a SO1020VP Combination Service Entrance Device Value Pack?

Value pack components

Product Line:
Combination Service Entrance Devices

CSED and branch breakers included in VP

Component parts

The SO1020VP includes
(1) SO1020M100S CSED, Ring type, 4-jaw meter socket, Overhead feed ONLY, Surface mount, with a 100amp Main breaker feeding a 10space-20circuit load center
(3) HOM120 (Homeline 20amp single pole branch circuit breaker)
(3) HOMT2020 (Homeline, 20amp Tandem single pole branch circuit breaker).

CTA-ID : 7776
Was this helpful?
What can we do to improve the information ?