Technical FAQs

Ask a Question

What is included in a CSEDVP1 Combination Service Entrance Device Value Pack?

Value pack components

Product Line:
Combination Service Entrance Devices 

CSED and branch breakers

Component parts

The CSEDVP1 includes
(1) SC3040M200S, which is a Ring type, 4-jaw meter socket, Overhead/Underground feed, Surface mount ONLY, with a 200amp Main Breaker feeding a 30space-40circuit load center interior. 
(2) HOM115 (Homeline, single pole, 15amp branch circuit breaker) 
(5) HOM120 (Homeline, single pole, 20amp branch circuit breaker)
(1) HOM250 (Homeline, two pole, 50amp branch circuit breaker).

CTA-ID : 7775
Was this helpful?
What can we do to improve the information ?