Technical FAQs

Ask a Question

What are the repair parts for a QO124M125RB, Series S1 (or S01), Load Center?

Issue:
Design repair parts

Product line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4054802209
Interior Trim - 4054507501
Interior Assembly - QO124M125RBI
Neutral Bonding Screw - 4028345850K
Main Circuit Breaker - QOM125VH
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screw - 2142717161
Main Circui Breaker and Main Lugs Keps Nut - 2342702001


CTA-ID : 7771
Was this helpful?
What can we do to improve the information ?