Technical FAQs

Ask a Question

What is the minimum load and maximum rating for the LOW LEVEL Connected/Closed Switch (EF) for the Masterpact NW breaker?<br /><br />

Low-level: 1 mA/4 V minimum load. Max. rating:
24/48 Vac 5 A
240 Vac 5 A
380 Vac 5 A
24/48 Vdc 2.5 A
125 Vdc 0.8 A
250 Vdc 0.3 A


CTA-ID : 8843
Was this helpful?
What can we do to improve the information ?