Technical FAQs

Ask a Question

What are the characteristics of the undervoltage trip for the Powerpact P-frame, R-frame, and NS630b - NS3200 electronic trip circuit breakers?

Characteristics
Vac 24, 48, 100/130, 200/250, 240/277, 380/480, 500/550
Vdc 12, 24/30, 48/60, 100/130, 200/250
Operating Threshold 0.7 to 1.1 Vn
Power Consumption (VA or W) Constant/Inrush 4.5/200
Breaker Response Time at Vn 50 ms ? 10


CTA-ID : 8833
Was this helpful?
What can we do to improve the information ?