Technical FAQs

Ask a Question

Are the clusters for the NW mounted on the breaker or on the cradle?

For UL/ANSI circuit breakers, the clusters are mounted on the circuit breaker;
for IEC circuit breakers, the clusters are mounted on the cradle.


CTA-ID : 8768
Was this helpful?
What can we do to improve the information ?