Technical FAQs

Ask a Question

What is the minimum load and maximum rating for the LOW LEVEL PF switch for the NT and NW breakers?<br /><br />

Low-Level: 1 mA/4 V minimum load. Max rating:
24/48 Vac 3 A
240 Vac 3 A
380 Vac 3 A
24/48 Vdc 3 A
125 Vdc 0.3 A
250 Vdc 0.15 A


CTA-ID : 8820
Was this helpful?
What can we do to improve the information ?