Technical FAQs

Ask a Question

What is the minimum load and maximum rating for the STANDARD PF switch for the NT and NW breakers?<br /><br />

Standard: 10 mA/24V minimum load. Max rating:
240/380 Vac 5 A
480 Vac 5 A
600/690 Vac 3 A
24/48 Vdc 3 A
240 Vdc 0.3 A
380 Vdc 0.15 A


CTA-ID : 8819
Was this helpful?
What can we do to improve the information ?