Technical FAQs

Ask a Question

How can you tell if a breaker with the new Micrologic trip unit is in overload pickup?

The trip unit includes an alarm indicator that will be lit continuously when the current is above 100% of the pickup setting.


CTA-ID : 7984
Was this helpful?
What can we do to improve the information ?