Technical FAQs

Ask a Question

What is the current rating for the 1a1b aux. switch on FD, FG, and FJ breakers?

Max. Load = 10 A @120 Vac 50/60 Hz


CTA-ID : 7751
Was this helpful?
What can we do to improve the information ?