Technical FAQs

Ask a Question

End user is connecting an AC sensor in a circuit and constantly getting flow to the solenoid. Is this correct?

The sensor has a leakage current at all times, for example 1.5 ma in the XS1M12FA260. Install a resistor between sensor and the solenoid to deenergize the solenoid when the sensor circuit is open, only bleed current present.


CTA-ID : 4897
Was this helpful?
What can we do to improve the information ?